Feb 03,2026 by T-Motor
T-MOTOR at UMEX 2026: Showcasing Advanced UAV Propulsion Systems
From January 20th to 22nd, the three-day UMEX 2026 concluded successfully at the Abu Dhabi National Exhibition Centre. As one of the largest and most influential professional drone exhibitions in the UAE, this year's event attracted over 380 leading companies from around the world, collectively showcasing cutting-edge unmanned systems solutions for a wide range of scenarios. T-MOTOR, a global leader in drone propulsion systems, participated in the exhibition with its core power products, including the A series, S series, and VZ series. With its leading technological expertise, T-MOTOR became one of the key highlights for visitors at the event.

1. X-A16L Coaxial Propulsion System
Designed for heavy-lift multi-rotor coaxial platforms, this system delivers a rated thrust of 70-75 kg per arm and a maximum thrust of 158 kg. Combining powerful load capacity with high reliability, it meets the demands of heavy-duty missions such as emergency firefighting, heavy logistics, and equipment lifting.


2. S-Series Propulsion System
Supporting high-voltage operation (400V/600V), this system achieves a single-motor maximum thrust range of 158-320 kg. It excels in professional applications including heavy logistics, specialized operations, and emergency rescue, delivering robust power support for heavy-lift aircraft.


3. VZ-Series VTOL Carbon Fiber Propellers
Engineered specifically for VTOL platforms, these propellers feature an optimized aerodynamic design coupled with high stiffness and lightweight characteristics. They effectively address the dual operational demands of VTOL takeoff/landing and cruise, offering a more powerful, durable, and lightweight propeller solution.

Beyond these highlighted products, T-MOTOR's booth also featured a comprehensive display of its broader portfolio, including the VL-series VTOL propulsion systems, AUZ-series fixed-wing carbon fiber propellers, and AT-series fixed-wing motors. This participation not only strengthened our relationships with existing partners but also enabled us to connect with numerous industry players in emerging markets, laying a solid foundation for future market expansion and technological collaboration.





Click to explore more UAV propulsion systems and solutions from T-MOTOR.