by shop.tmotor

Common Drone Propulsion Issues and How to Fix Them

Common problems and solutions for drone propulsion systems

If your drone is flying unstably or lacks sufficient power, the problem is often with the UAV propulsion system, also known as the UAV power system.. Whether you're a professional drone pilot or an amateur aerial photography enthusiast, understanding common drone propulsion problems and their solutions can be very helpful. This article will guide you step-by-step through troubleshooting, from the drone's motors, ESCs, and propellers to overall tuning, helping you maintain stable and safe power output for your drone.

Drone Motor Problems and Solutions

The motor is the core of a drone — and in many cases, the core of the UAV propulsion system — so even small issues can lead to unstable flight or power loss.

Drone Motor Overheating During Flight

Drone motor overheating is one of the most common UAV motor issues, especially during long hovering or heavy-load flight.

Drone Motor Overheating Solutions:

  • First, ensure your drone's motor, ESC, and battery are properly matched.With T-MOTOR matched UAV propulsion kits, all motors, ESCs, and propellers come pre-selected and ready to fly
  • Then, check if the motor shaft or air duct is blocked by foreign objects.
  • Finally, try to avoid prolonged high-load flight. If necessary, you can add heat sinks or improve the body's ventilation.

Insufficient Drone Thrust and Slow Climb Performance

If your drone struggles to climb or feels sluggish when increasing throttle, this is often one of the earliest signs of insufficient propulsion thrust.

Drone Thrust and Slow Climb Solution:

  • First, check if the motor and propeller are properly matched, and if the KV value and propeller size are appropriate.
  • Then, clean the motor bearings and shaft to ensure smooth rotation.
  • Finally, test the ESC output to see if there are any voltage drops or current limitations.

Drone ESC Problems and Troubleshooting Solutions

The ESC controls motor speed, and its condition directly affects drone flight stability and overall UAV power management.

Overcurrent Protection Triggered

If the ESC frequently enters overcurrent protection mode, it means the current exceeds the safe range, triggering the overcurrent protection.

Consequences: The ESC limits or cuts off the current output to prevent the motor and ESC from burning out due to overload, but this may be accompanied by chain reactions such as motor stoppage, power interruption, and loss of flight control. In severe cases, it can lead to a crash.

How to reduce the risk of overcurrent protection triggering:

Properly match ESC and motor parameters.

The continuous current value of the ESC should be greater than the maximum operating current of the motor (a 20%-30% margin is recommended).

Avoid using high KV motors with low-voltage batteries to prevent excessive current demand.

Use ESCs with protection functions.

Choose ESCs that support multiple protections such as overcurrent, overheating, and low voltage to improve safety.

High-end ESCs (such as those supporting the DShot protocol) have faster response speeds, which can reduce the power interruption time when protection is triggered.

Signal Interference

ESCs are very sensitive to signals. Interference can cause the motor speed to fluctuate, and signal interference can also cause the motor to stop. The remaining motors then have to bear a greater load, potentially leading to power distribution imbalance, causing the aircraft to tilt, roll, or even crash.

Solutions:

  • Use shielded wires or reroute the wiring to avoid interference. Or simplify the process entirely with a T-MOTOR pre-matched propulsion kit where the ESC and motor are already perfectly compatible.
  • Regularly check key components (such as capacitor capacitance and heatsink temperature rise) and replace aging components promptly.
  • Try changing the frequency band or flying away from the interference source.

Drone Propeller Vibration Problems and Causes

Propellers not only determine thrust output, but also play a major role in drone vibration control and overall flight stability.

Uneven Mass Distribution

During the manufacturing process, propellers may experience uneven mass distribution due to uneven materials, processing errors, or wear, cracks, or deformation after long-term use.

Installation Problems

  • Incorrect direction: Installing the propeller in the wrong direction will lead to abnormal lift direction and cause vibration.
  • Uneven screw tightness: If the propeller fixing screws are not tightened to the standard value (e.g., 0.6-0.8 N·m) using a torque wrench, it may cause additional vibration during propeller rotation.

Solutions:

  • Regularly check the propellers for wear. Choosing a T-MOTOR matched propulsion kit ensures you get pre-balanced propellers that meet ISO standards, reducing vibrations.
  • Measure the vibration amplitude and angle in the rotating state using vibration detection equipment (such as a propeller balancer) to determine the imbalance, and correct it by adding counterweights (such as tape, glue, etc.).
  • Select pre-balanced propellers that meet ISO standards to reduce vibrations caused by manufacturing defects.

Correct Installation Method

Installing the propeller in the wrong direction will lead to abnormal lift direction and significant flight vibration, even thrust imbalance.

Points to note:

  • Each propeller must be installed according to the marked direction.
  • The screws should be tight, but not too tight, to prevent the propeller from bending.
  • After installation, perform a low-speed test flight first, then gradually increase the flight speed.

Integrated Debugging Techniques for UAV Propulsion Systems

Integrated debugging of UAV propulsion systems should focus on the motor, propeller, ESC (Electronic Speed ​​Controller), battery, and flight control system. Troubleshooting individual problems is important, but overall system debugging should not be neglected.

Data Recording and Analysis:

  • Record key data during the debugging process, including motor speed, current, battery voltage, and temperature rise.
  • Generate a debugging report, noting performance differences before and after debugging, to provide a reference for subsequent optimization.

Problem Troubleshooting and Resolution:

  • If any abnormalities are found during debugging, immediately stop the test and investigate the cause.
  • Based on the problem symptoms and data analysis results, take targeted measures to resolve the issue.

Continuous Optimization and Improvement:

  • Continuously optimize and improve the UAV propulsion system based on debugging results and flight test feedback.
  • Adjust parameter settings, replace components, or improve the design to enhance UAV performance and stability.

While UAV propulsion systems may seem complex, mastering these common troubleshooting methods, combined with official tools and data monitoring, can quickly resolve most faults. Paying attention to details, avoiding high loads, and performing timely maintenance will lead to smoother and safer flights, and fewer frustrating unexpected problems.